EEPROM protection when flashing mcu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM protection when flashing mcu

Jump to solution
1,840 Views
Iko
Contributor II

Hi all.

I'm working on Mc9S08DZ60.

 

I want to flash my MCU whitout erase eeprom.

I have seen the "BDM_P&E_Multilink_CyclonePro.ini", and i had write "1" to prevent eeprom:

 

[9S08DZ60]
PROGRAMMING_ALGORITHM=0
DOTRIM=1
PRESERVE1_START=0
PRESERVE1_END=0
PRESERVE1_ACTIVE=0
PRESERVE2_START=0
PRESERVE2_END=0
PRESERVE2_ACTIVE=0
PRESERVE3_START=0
PRESERVE3_END=0
PRESERVE3_ACTIVE=0
PRESERVE_EEPROM=1
CUSTOM_TRIM=0
NGS_TRIM_OVERRIDE_REFERENCE_FREQUENCY=3126500

 

 

But it seems to have no effect...

How i can do to prevent my eeprom?

 

Ty all

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,433 Views
CrasyCat
Specialist III

Hello

 

Just select "Advanced programming/Debugging Options" in the Multilink/CyclonePro menu and then indicate the memory areas you want to keep as is in the "Non volatile memory Preservation" group.
You can also take a look at following thread:

CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,434 Views
CrasyCat
Specialist III

Hello

 

Just select "Advanced programming/Debugging Options" in the Multilink/CyclonePro menu and then indicate the memory areas you want to keep as is in the "Non volatile memory Preservation" group.
You can also take a look at following thread:

CrasyCat

0 Kudos
Reply