Downloading to 1321X-SRB using "Test Tool".

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Downloading to 1321X-SRB using "Test Tool".

跳至解决方案
2,203 次查看
stuartgw
Contributor I
Hi,

I am trying to write an app for the 1321X-SRB. I have used Code Warrier to build the app and am trying to download the S-record file using Test Tool.

I always get the error mismatch found on address=0xFFFE.

Is there some setting I have to change to get this to work? I'm assuming that I should select "HCS08 Serial Monitor" in code warrier?

I can download the pre-compiled example apps, but not anything I compile.

Any help appreciated,

Stuart
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
738 次查看
CompilerGuru
NXP Employee
NXP Employee
Not sure how much I can help you here as I dont know (or own :smileyhappy: a 1321X-SRB board.
Anyway, the error you get is about the reset vector, which is specified in the prm file with "VECTOR 0 _Startup".
If you uncomment this line, you probably will be able to flash it, but then the question is, how does you app start? Is there another vector address to use instead?
(if so, use VECTOR ADDRESS 0xABCD _Startup)
Well I just dont know.

Daniel

PS: The serial monitor does actually map the reset vector to another address than 0xFFFE, but it does automatically perform this remapping while downloading, as far as I known.

在原帖中查看解决方案

0 项奖励
回复
1 回复
739 次查看
CompilerGuru
NXP Employee
NXP Employee
Not sure how much I can help you here as I dont know (or own :smileyhappy: a 1321X-SRB board.
Anyway, the error you get is about the reset vector, which is specified in the prm file with "VECTOR 0 _Startup".
If you uncomment this line, you probably will be able to flash it, but then the question is, how does you app start? Is there another vector address to use instead?
(if so, use VECTOR ADDRESS 0xABCD _Startup)
Well I just dont know.

Daniel

PS: The serial monitor does actually map the reset vector to another address than 0xFFFE, but it does automatically perform this remapping while downloading, as far as I known.
0 项奖励
回复