Down grade Codewarrior IDE from V4.7 to V4.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Down grade Codewarrior IDE from V4.7 to V4.5

Jump to solution
2,093 Views
sebikoo
Contributor I
Hello, All freescaler worldwide
 
 
I am having compile erros to complie a project made by V4.5 evaluation version 
 
at V4.7 evaluation version Thus, I have received license.dat file for V4.5 evaluation version
 
 from technical support center recently.
 
 
I currently do not have V4.5 evaluation version installation file, but only V4.7 evaluation version 
 
installation file. How could I change it to V4.5 with license.dat file received ?
 
 
Best Regards..
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,104 Views
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish

View solution in original post

0 Kudos
Reply
2 Replies
1,105 Views
stanish
NXP Employee
NXP Employee
Hello sebikoo

I'd recommend you to use rather newer version since it fixes several defects.
Could you possibly specify more in detail which errors do you get?

Anyway, if you insist on v4.5 you can open Service Request and the support will send you the installer.

Stanish
0 Kudos
Reply
1,104 Views
sebikoo
Contributor I
Hello Stanish
 
Errors are solved. By the way, I might face with other errors for the next weeks, because
 
this project has not been mine but others'
 
So, pls keep touch in me for later.
 
Thanks anyway for your help on this.
 
 
Regards.
0 Kudos
Reply