Hello Karima
The free downloading CodeWarrior can be Evaluation Edition or Special Edition.
The former works same as professional edition, but it has 30-day time restriction.
The latter has no time restriction, but it has C code size limit, for the restriction of different CodeWarrior editions, please refer to:
http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf
If you have problem to find out whether your license is Special license, or Evaluation license, please attach it in this thread, I will check it.
The license file is placed under CodeWarrior installation folder, e.g,
C:\Program Files (x86)\Freescale\CWS12v5.1
C:\Freescale\CW MCU v10.6.4\MCU
Best Regards
Fiona Kuang
TIC - Technical Information Center
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------