Difference between the free and paid version of CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between the free and paid version of CodeWarrior

1,198 次查看
karimaaissaoui
Contributor II

Hello everyone I wonder if I'm working with a version of CodeWarrior unlicensed download by net, can cause me problems during the compilation of a code indicating that the RAM is insufficient.

Thank you very much in advance for your support.

标签 (1)
0 项奖励
回复
2 回复数

1,017 次查看
karimaaissaoui
Contributor II

Thank you very much for your reply.

I will like to find out if it's possible, the max size memory tolerated for CodeWarrior as a trial version.

Thank you in advance.

0 项奖励
回复

1,017 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Karima

The free downloading CodeWarrior can be Evaluation Edition or Special Edition.

The former works same as professional edition, but it has 30-day time restriction.

The latter has no time restriction, but it has C code size limit, for the restriction of different CodeWarrior editions, please refer to:

http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/950-00437.pdf

If you have problem to find out whether your license is Special license, or Evaluation license, please attach it in this thread, I will check it.

The license file is placed under CodeWarrior installation folder, e.g,

C:\Program Files (x86)\Freescale\CWS12v5.1

C:\Freescale\CW MCU v10.6.4\MCU

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复