Difference between CW6.0 and 6.1 for HCS08?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between CW6.0 and 6.1 for HCS08?

Jump to solution
2,407 Views
Lundin
Senior Contributor IV
I have been trying to dig up some patch notes regarding what differences there are between CW6.0 for HCS08 and CW6.1, without success.

If anyone has the link to the documentation or can give me a brief review of 6.1, that would be much appreciated.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,107 Views
CrasyCat
Specialist III
Hello
 
Attached the Welcome_CW_MCUs.txt file from V6.1, which should provide high level summary of changes between V6.0 and V6.1.
 
CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
1,108 Views
CrasyCat
Specialist III
Hello
 
Attached the Welcome_CW_MCUs.txt file from V6.1, which should provide high level summary of changes between V6.0 and V6.1.
 
CrasyCat
0 Kudos
Reply
1,107 Views
Lundin
Senior Contributor IV
Thank you.
0 Kudos
Reply