Debug and Mon08_Interface.ini for M68DEMOQTY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug and Mon08_Interface.ini for M68DEMOQTY

Jump to solution
3,435 Views
JM
Contributor I

In Code Warrior V5.7.0
for an assembly project created using M68HC908QT4 chip

When Debug is called, I always have to choose a device.

Is there a way to skip the <Choose Device> window ?

Also, switching from Mon08 Interface to Full Chip Simulation and back to Mon08

Interface always result in loosing connection configuration. So each time I have to

add a connection, change baud rate, change device, exit Debug, reenter Debug, choose device and connect.

Is there a way for Debug to look at the configuration file Mon08_Interface.ini and use the connection configuration and device description ?
What would be the instructions to insert in the configuration file ?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,282 Views
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

View solution in original post

0 Kudos
Reply
1 Reply
1,283 Views
FC
Contributor III

Do you have the right monitor program, there is an error supplied with the demo board.  Go to www.hc08.cz, it has good information on the 908qt4 (Nitron) mcu. 

0 Kudos
Reply