Convertion from >DIR to .mov

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Convertion from >DIR to .mov

ソリューションへジャンプ
1,616件の閲覧回数
viji
Contributor I
Hi there,

Is there any way to convert .DIR and respective .AUD files to QT movie file?
I have a set of .DIR and .AUD files, which I want to play using Quicktime player.

Thanks for any help.

Viji

Message Edited by viji on 2007-06-25 05:27 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
639件の閲覧回数
J2MEJediMaster
Specialist I
You're talking about converting media files for QuickTime. I'm not sure this is the appropriate forum for this, as CodeWarrior tools are oriented towards embedded work now. You want to go to the Apple Developer forums at http://developer.apple.com/, or alternately, Google for media convertor utilities.

---Tom

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
639件の閲覧回数
CrasyCat
Specialist III
Hello
 
I am not sure you are on the appropriate Forum here.
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
CrasyCat
0 件の賞賛
返信
640件の閲覧回数
J2MEJediMaster
Specialist I
You're talking about converting media files for QuickTime. I'm not sure this is the appropriate forum for this, as CodeWarrior tools are oriented towards embedded work now. You want to go to the Apple Developer forums at http://developer.apple.com/, or alternately, Google for media convertor utilities.

---Tom
0 件の賞賛
返信