Content of a .CRT file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Content of a .CRT file

1,792 Views
FabioPdM
Contributor I

Hi, 

I have some static bytes in the source file like a stamp.

When I search for this stamp in the .crt file that will be loaded in the MC it does not exist.

Any one could help me?

0 Kudos
Reply
4 Replies

1,745 Views
FabioPdM
Contributor I

Hi Alice,

    In time, I forgot to mention that this .CRT file have 0x0D 0x0A record separators.

    Could be that this file a Freescale SRecord format?

    If so I can create it again with CW easily!!!

0 Kudos
Reply

1,757 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @FabioPdM 

For better help you, please tell us the part number of your MCU, thanks.

 

 

BR

Alice

0 Kudos
Reply

1,747 Views
FabioPdM
Contributor I

Hi Alice,

      The target is MCU MC9S08AW32 and to burn it  they use a .CRT file extension that I dont know how it is created and file format.

       That's the reason that I am investigating how this file extension was created to solve the doubt.

       This file extension .CRT give any clue how can I generate it in the CW?

       The first 16 bytes in the .CRT file are ( hex 0x ) 61 69 73 64 7F 7D 43 5A 43 5D 5D 5F 44 47 5B 5E 6F 5E 73 42 ( 'aisd' )    .

       Thanks for your help!!!

0 Kudos
Reply

1,719 Views
Itzzamna_Supp
NXP TechSupport
NXP TechSupport
When compiling, S19 is generated and remains in the FLASH folder, the SRecord file type is saved there in S19, where you will find the CRT.
0 Kudos
Reply