Confusion on how to update my compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusion on how to update my compiler

ソリューションへジャンプ
2,214件の閲覧回数
Luigi
Contributor III
I am using Codewarrior IDE, version 5.7.0, build 2015.  I need to get the header file for the 'AC16 processor.  I went to the downloads page, and it shows "Updates for CodeWarrior for HC(S)08/RS08 v5.1".  But I am running 5.7.0, so what do I download?  Thanks in advance.
 
Lou
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,154件の閲覧回数
stanish
NXP Employee
NXP Employee
Hi Lou,

The version you refer to is just IDE version. In order to get product version you should press "Installed Products" button in the About dialog.
IDE version 5.7.0 build 2015 corresponds to  CodeWarrior v5.1. You can download AC16 Service Patch here:

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=HC08-V5-1-AC16-SP&nodeId=0127260061...


Stahish

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,155件の閲覧回数
stanish
NXP Employee
NXP Employee
Hi Lou,

The version you refer to is just IDE version. In order to get product version you should press "Installed Products" button in the About dialog.
IDE version 5.7.0 build 2015 corresponds to  CodeWarrior v5.1. You can download AC16 Service Patch here:

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=HC08-V5-1-AC16-SP&nodeId=0127260061...


Stahish
0 件の賞賛
返信
1,154件の閲覧回数
Luigi
Contributor III
Thank you!
0 件の賞賛
返信