Complex type CW MCU 10.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Complex type CW MCU 10.2

2,542 次查看
ioanacroitoru
Fresh Out Contributor

Hello,

 

I need to use a complex type in order to see the result returned by std::polar.

I see that the CW10.2 contains <complex.h> with the next definition:

 

#define complex      _Complex;

 

complex is not recognized like a type but _Complex apperas to be a type(the style it's the same as a int or void). Yet I get next error:

 

undefined identifier '_Complex' ;

 

What can I use for a complex number if that is not correct?

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

2,344 次查看
carlos_neri
NXP Employee
NXP Employee

Have you tried to add C99 support on CW compiler options?

I think complex data type was integrated to C on C99 revision. For default, CW uses C without C99 , if you want C99 support you need to enable it on the compiler options.

2,344 次查看
hebo
Contributor I

Hi,

I  met the same problem, How to set C99 support on the compiler options,

0 项奖励
回复

2,344 次查看
ioanacroitoru
Fresh Out Contributor

Hi,

First thank you for your answer.

Now I get the error

     "complex types are not implemented"

I'm guessing that I can't use complex type alter all? Or what does this means?

0 项奖励
回复

2,344 次查看
carlos_neri
NXP Employee
NXP Employee

Not sure which MCU device you're using, but here is my findings:

It seems the Freescale ARM compiler does not supported, need to double check that (got the same result as you).

I did the same test with GCC compiler within CW10.4 and it seems it supports it. Probably if your application allows it, you could move to GCC compiler using CW10,4?

0 项奖励
回复