I have never used CodeWarrior but I have a need for it. I have CodeWarrior 10.1.1 targeting a P2040 running Linux with a USB JTAG TAP installed. The board is occasionally locks up under certain conditions. What I want to do is boot the board from flash wait for it to lock up, then break in with CodeWarrior and dump the registers, most importantly the program counter.
I don't see anything in the user documentation on how to do this. I don't need to develop and download code. I only want to dump the registers when the board locks up. Can someone tell me if there is a simple way to do this?