In the new CW 10.5 there is now the possibility to import a project created with CW for DSC v. 8.3 .
The import utility runs quite well ( just some minor problems with some linker directives but quite easy to solve ) .
But when i build the project in CW10.5 I get a total size of the code about 5% greater compared to the code size i've got with the same project in CW8.3 ..
Has anyone already seen this behavior ? Any solutions ?
解決済! 解決策の投稿を見る。
There's some change in 56800E compiler to fix the known bugs and improve the efficiency. So it is possible that the code size afte building is changed. If code size is quite important for you, please enable the optimazation globally or locally.
There's some change in 56800E compiler to fix the known bugs and improve the efficiency. So it is possible that the code size afte building is changed. If code size is quite important for you, please enable the optimazation globally or locally.