Code size growth in CW 10.5 DSC Compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code size growth in CW 10.5 DSC Compiler

Jump to solution
1,065 Views
GottiLuca
Contributor IV

In the new CW 10.5 there is now the possibility to import a project created with CW for DSC v. 8.3 .

The import utility runs quite well ( just some minor problems with some linker directives but quite easy to solve ) .

But when i build the project in CW10.5 I get a total size of the code about 5% greater compared to the code size i've got with the same project in CW8.3 ..

Has anyone already seen this behavior ? Any solutions ?

Labels (1)
0 Kudos
Reply
1 Solution
916 Views
TICS_Fiona
NXP Employee
NXP Employee

There's some change in 56800E compiler to fix the known bugs and improve the efficiency. So it is possible that the code size afte building is changed. If code size is quite important for you, please enable the optimazation globally or locally.

View solution in original post

0 Kudos
Reply
1 Reply
917 Views
TICS_Fiona
NXP Employee
NXP Employee

There's some change in 56800E compiler to fix the known bugs and improve the efficiency. So it is possible that the code size afte building is changed. If code size is quite important for you, please enable the optimazation globally or locally.

0 Kudos
Reply