Code in Runtime.PPCEABI.VS.UC.a, and how to get them?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code in Runtime.PPCEABI.VS.UC.a, and how to get them?

1,107 Views
qinruirose
Contributor I

Hi, all, How can I know the code/files in runtime libraries(Runtime.PPCEABI.VS.UC.a), and how can I get them? Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

905 Views
TICS_Fiona
NXP Employee
NXP Employee

Dear customer,

The "Runtime.PPCEABI.VS.UC.a" is the runtime libraries for MPC55xx and MPC56xx products. You can find this library under CodeWarrior v2.10 installation directory:

installDir\PowerPC_EABI_Support\Runtime\Lib

Along with the pre-built runtime libraries, this CodeWarrior product includes the source

code and project files required to build the runtime libraries.

All runtime library source code files are in this directory:

installDir\PowerPC_EABI_Support\Runtime\Src

The runtime library project files are in this directory:

installDir\PowerPC_EABI_Support\Runtime\Project

The project names are Runtime.PPCEABI.mcp and Run_EC++.PPCEABI.mcp.

Each project has a different build target for each configuration of the runtime library. For more information about customizing the runtime libraries, read the comments in the source code files as well as the runtime library release notes.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply