Code Warror 10.3 post-build "The syntax of the command is incorrect."

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warror 10.3 post-build "The syntax of the command is incorrect."

939 Views
johnreynolds
Contributor II

Hi, I get this error kicked out of the console after running my post-build windows cmd script. It's seems to be a Windows 7 command line error, like when you try to copy files with embedded spaces etc. I can run my cmd script from the command line with no error, even checking that %errorlevel% is zero. Everything works except this annoying message at the end. If I remove the post-build entry, I do not get the error. The "All Done!" is echoed from the cmd script. After that CW10.3 takes over.

 

Thanks,

John Reynolds

 

.

.

.

C:/Freescale/CW MCU v10.3/gnu/bin/mingw32-make --no-print-directory post-build

'Generate CRC and append to .rbin '

MQXbootPost      C:/Freescale/Freescale_MQX_4_0/demo/Windchime\twrcf52259_Int_Flash_Bootloader_Debug     Windchime.elf.rbin

Windchime.elf.rbin is 524288 bytes

Read 516094 bytes starting at 0x2000. CRC=0xEFA6

03:41 PM

All done!

' '

The syntax of the command is incorrect.
Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

759 Views
Rick_Li
NXP Employee
NXP Employee

Hi John,

could you please post your script in this thread for investigating?

if possible, could you please also post your project here also?

0 Kudos
Reply