Changing processor for a CW10.4 project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Changing processor for a CW10.4 project?

跳至解决方案
1,193 次查看
frankvanhooft
Contributor III

Apologies for the newbie question. Using CW10.4 under Windows I've imported the project for AN4370 (USB bootloader for the K20) and it's building fine. I need to actually target the KL25 processor. I understand I need to change the linker file. But how do I change the target processor? I see in the project properties it's saying Cortex-M4, but where can I change it to Cortex-M0?  (And is there anything else I should be doing?)

 

Thanks a lot.

标签 (1)
0 项奖励
回复
1 解答
1,055 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

in CW10.2 and other past version, there is MCU Change Wizard. however CW10.3 and CW10.4 doesn't have MCU Change Wizard. It was removed. Because: - it only worked for simple cases - Customers tried unsuccessfully to use this wizard to change the target connection. This was NOT the intended purpose. our recommendation is to create a new CW MCU v10.4 project and drag ‘n drop files into the project

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,056 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

in CW10.2 and other past version, there is MCU Change Wizard. however CW10.3 and CW10.4 doesn't have MCU Change Wizard. It was removed. Because: - it only worked for simple cases - Customers tried unsuccessfully to use this wizard to change the target connection. This was NOT the intended purpose. our recommendation is to create a new CW MCU v10.4 project and drag ‘n drop files into the project

0 项奖励
回复
1,055 次查看
frankvanhooft
Contributor III

Thanks for the response. I might not be too excited about the answer (more work for me), but I'm impressed by the fast response. Thanks very much.

0 项奖励
回复
1,055 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!

0 项奖励
回复