Cant save Settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cant save Settings

1,395 Views
SecondTechCo
Contributor IV

Using code warrior 10.2 and for some reason, we cant seem to save settings.   This is occurring on multiple machines.    We try to add a header or source  folder using project-properties-coldfire compiler-Input   so that these are included in the project.  This works fine and the project compiles just fine.  If we close the project and reopen, the folder is then gone from the list.  Any help would be greatly appreciated.

Labels (1)
0 Kudos
Reply
3 Replies

1,251 Views
Rick_Li
NXP Employee
NXP Employee

this issue should be a defect of Linux version CodeWarrior, and Freescale will not release further CW version based on Linux system after 10.2.

I'm sorry for this inconvenience has caused to you!

0 Kudos
Reply

1,251 Views
SecondTechCo
Contributor IV

This was determined to be a linux based backup systems which changes the file attribute on the .project file to be hidden.   Linux and Western Digital dont handle files without names well and eclipse doesn't display good error messages when the file is hidden.

I don't possible know why eclipse stores 3 files in the project with just an extension and not a name any way.

0 Kudos
Reply

1,251 Views
SecondTechCo
Contributor IV

We also seem to have problems with the debug configurations randomly being forgotten by eclipse and we have to recreate them.  Not sure if these two things are related but they are frustrating.

0 Kudos
Reply