Cannot connect to DEMO9S08QG8 demo booard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot connect to DEMO9S08QG8 demo booard

ソリューションへジャンプ
3,007件の閲覧回数
FC
Contributor III
I cannot connect to the DEMO9S08QG8 demo board.  I gives an error saying "Target running".  All the jumper settings are correct.
 
Any ideas?
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,078件の閲覧回数
FC
Contributor III
The debugger locks up.  This happens both on V3.1 and V5.0.   The driver is loaded fine.  I am running windows xp sp2 home edition.  Tech support has told me that windows xp home edition is no compatible.  I find this hard to believe. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,079件の閲覧回数
FC
Contributor III
The debugger locks up.  This happens both on V3.1 and V5.0.   The driver is loaded fine.  I am running windows xp sp2 home edition.  Tech support has told me that windows xp home edition is no compatible.  I find this hard to believe. 
0 件の賞賛
返信
1,078件の閲覧回数
KLawrence
Contributor I
Are you sure you're connecting with the P&E BDM target (or some target with BDM in the title)?
0 件の賞賛
返信