Cannot connect to DEMO9S08QG8 demo booard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot connect to DEMO9S08QG8 demo booard

Jump to solution
2,989 Views
FC
Contributor III
I cannot connect to the DEMO9S08QG8 demo board.  I gives an error saying "Target running".  All the jumper settings are correct.
 
Any ideas?
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,060 Views
FC
Contributor III
The debugger locks up.  This happens both on V3.1 and V5.0.   The driver is loaded fine.  I am running windows xp sp2 home edition.  Tech support has told me that windows xp home edition is no compatible.  I find this hard to believe. 

View solution in original post

0 Kudos
Reply
2 Replies
1,061 Views
FC
Contributor III
The debugger locks up.  This happens both on V3.1 and V5.0.   The driver is loaded fine.  I am running windows xp sp2 home edition.  Tech support has told me that windows xp home edition is no compatible.  I find this hard to believe. 
0 Kudos
Reply
1,060 Views
KLawrence
Contributor I
Are you sure you're connecting with the P&E BDM target (or some target with BDM in the title)?
0 Kudos
Reply