Hi,
I tried some demos from CW 10.6 and KDS 3.0 on the FRDM-KE02Z (Bootloader: V1.11 & App.Vers.: 1.14).
I used OpenSDA Embedded Debug-USB Port from CW 10.6 Trial.
I can flash and run the elf codes without problems.
The hex-codes, generated simultaneously with the elf-codes and flashed the same way, don't run.
I need some help
hi,
how do you flash hex file to target? via simple flash tool "Flash to Target"?
please make sure you didn't use _host related library in your project:
if this can't help, please specify the steps to reproduce the problem step by step with your demo code.
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------