Can not import K60N512 project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not import K60N512 project.

ソリューションへジャンプ
904件の閲覧回数
danielchai
Senior Contributor I

Hi All,

I just installed the MQX3.8.1 patch for GS1500M. When I follow the instruction to import the project httpsrv_twrk60n512 from  rtcs\examples\gstwr_httpsrv. It gives me error:


Error processing changed links in project description file.

Details:

No file system is defined for scheme:

 

Any ideas about this?

 

Thanks.


ラベル(1)
0 件の賞賛
返信
1 解決策
796件の閲覧回数
danielchai
Senior Contributor I

I found the problem.

The MQX_ROOT_DIR setting in the demo project is wrong.

The project is based on MQX3.8.1 but the MQX_ROOT_DIR is set to MQX3.7.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
797件の閲覧回数
danielchai
Senior Contributor I

I found the problem.

The MQX_ROOT_DIR setting in the demo project is wrong.

The project is based on MQX3.8.1 but the MQX_ROOT_DIR is set to MQX3.7.

0 件の賞賛
返信