Can codewarrior for MCU V10.6 flash MC9S08AC60 and MC9S08PA60?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can codewarrior for MCU V10.6 flash MC9S08AC60 and MC9S08PA60?

2,245件の閲覧回数
zhouzhuoqiang
Contributor I

Codewarrior for MCU V6.0 can't flash MC9S08PA60, as there isn't service pack for MC9S08PA60 in codewarrior for MCU V6.0. Can V10.6 flash MC9S08PA60?

 

 

 

Thanks a lot!

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,831件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

unfortunately MC9S08PA/PT devices can be only supported under CW10.

you can use CW10.6 to edit/buiild/debug/program MC9S08PA60.

if you want to program MC9S08PA60 in standlone mode, please refer this url:

https://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

can this help you?
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,831件の閲覧回数
zhouzhuoqiang
Contributor I

Hi,

Where can I download Service Pack: CW MCU V6.0 for MC9S08AC60 and MC9S08PA60?

Best regard

0 件の賞賛
返信

1,831件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

all CW for MCU v6.0 service packs are listed here

CodeWarrior Updates for MCUs v6.0|NXP

from where we can see there is no MC9S08AC60 pack for CW MCU v6.0. CodeWarrior for Microcontrollers v6.0 - AC16 Service Pack can support MC9S08AC16/8 but can't support MC9S08AC60 device.

to work with MC9S08AC60 you can use latest eclipse CW10.6.4  or classic CW6.3. here is the download link

Special Edition Software|NXP

can it help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,831件の閲覧回数
zhouzhuoqiang
Contributor I

Hi, Zhang,

I installed classic CW6.3 in 32bit Windows XP, and try to flash s19 file to MC9S08AC60.

The operation step is: Hi-wave--->File--->Open configuration---->E2006_touch.ini. At this moment, an error occurred. The details is " An error occurred when executing command file: E2006_touch.hwl"

0 件の賞賛
返信

1,831件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello,

this question was answered

Classic CW 6.3


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信