Hello
This seems to be related to your project.
I did open a couple of project created with V3.1 and I could build them in V4.6 without any trouble.
Also there are not enough information to help you more.
I would recommend you the following:
Generate the preprocessor listing for the start12.c file in V3.1 and check where the typedef is defined there...
If this does not help, I would recommend you to submit a service request for that.
Click
here to submit a service request.
Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.
Attach the generated .zip file to the SR.
CrasyCat