[CW3.1 S12A128] Can ANYBODY tell me that this works?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[CW3.1 S12A128] Can ANYBODY tell me that this works?

Jump to solution
2,232 Views
mke_et
Contributor IV
I don't really know if this is a CW issue or a hardware issue with the part.  I'm using the CW3.1 SE that comes with the USB BDM pod to program a 9S12A128.
 
Has ANYBODY been able to make the memory display windows in the CW Debugger display updated FLASH page data?  I'm trying to debug routines that reprogram the flash at a 'switched in page', and CW won't update.  I can see the 'original' data in the flash if I go out to it's 'real' address (388000h in this case) but it never changes.
 
I've spent a week and a half chasing down issues associated with this, and at this point if I'm told it won't work I'll just have to move 'around' the issue.  I can't spend any more time on it.

Message Edited by Alban on 02-23-2006 02:38 PM

Labels (1)
Tags (1)
0 Kudos
1 Solution
650 Views
desroc01
Contributor II
I am using the 9s12badge (MC9S12DP256) from Future. I also use the USB multilink (rev b 105) and everything works fine in CW 3.1

Check you target. You have to target the flash and not the simulator.

check this website.. there is a "frame project" that target the flash for the 9S12DP256

http://www.futureerc.com/9s12resource/9S12BADGE/9S12BADGE_index.htm

Good luck

View solution in original post

0 Kudos
1 Reply
651 Views
desroc01
Contributor II
I am using the 9s12badge (MC9S12DP256) from Future. I also use the USB multilink (rev b 105) and everything works fine in CW 3.1

Check you target. You have to target the flash and not the simulator.

check this website.. there is a "frame project" that target the flash for the 9S12DP256

http://www.futureerc.com/9s12resource/9S12BADGE/9S12BADGE_index.htm

Good luck
0 Kudos