CW10 mystery error - missing ProcessorExpert.obj file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CW10 mystery error - missing ProcessorExpert.obj file

跳至解决方案
3,952 次查看
JakeP
Contributor I

I have a project in CW10 and I had it working the last time I had CW10 running, as in it built clean and debugged successfully.  It's been a couple weeks and I just opened the project back up to continue working on it, and now when I try to build it's spitting out the following errors:

 

Cannot open file ./Sources/ProcessorExpert.obj

make: *** [SLP_2.abs] Error 1

Symbol 23 - error duplicated in ProcessorExpert.obj and Events.obj

 

The only changes that I've made since last opening the project was some basic additions to the source code.  I didn't do anything with processor expert config, project config, beans, etc.  The files ProcessorExpert.obj and Events.obj are listed in the project file tree under MC9S08GB60/Sources where they should be.  Seems like one of those ghost issues where you get something working then let it sit for a while and then it's mysteriously broken when you come back to it...

 

I've had this problem before with other projects and I could never figure out whats going on.  In the past I've had to recreate the entire project to be able to move forward.

 

Does anyone know the cause of the problem I'm seeing and how to resolve it?

 

Thanks!

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,191 次查看
CompilerGuru
NXP Employee
NXP Employee

When adding this line to main.c and a newly created file s.c

> int defined_twice=2;

 

I get these errors in the problems view:

 

Cannot open file ./Sources/s.obj s08 line 0 C/C++ Problemmake: *** [s08.abs] Error 1 s08 line 0 C/C++ ProblemSymbol 14 - defined_twice duplicated in s.obj and main.obj s08 line 0 C/C++ Problem

 

The problems view sorts them by the description, which is a bit unfortunate as the last one actually caused the two other messages. Also the "Cannot open file" is a bit misleading, as it can open it, the linker just does not like the content.

 

Just added this to show that the error in the original report just is a variable or function name and not part of the message.

 

Daniel

 

在原帖中查看解决方案

0 项奖励
回复
10 回复数
3,191 次查看
JakeP
Contributor I

A little more info...  I cleaned the project and rebuild the processor expert code and it had no effect.  Restarted my PC and CW10 for the heck of it and still no go.

0 项奖励
回复
3,189 次查看
BlackNight
NXP Employee
NXP Employee

Could you post your full Console Log output? Or even better: your project?

 

BK

0 项奖励
回复
3,189 次查看
JakeP
Contributor I

I do appreciate the help but at this time I won't be able to post the whole project because of IP protection concerns.

Here's PART 1 (because of msg post char limits) of the console output after a clean+build right after opening CW:

 

 

HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/Led.c'
' '
'Building file: ../Generated_Code/PE_Timer.c'
'Invoking: HCS08 Compiler'
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PE_Timer.args" -ObjN="Generated_Code/PE_Timer.obj" "../Generated_Code/PE_Timer.c"
../Generated_Code/PE_Timer.c
Command Line: '-ArgFile"Generated_Code/PE_Timer.args" -ObjN="Generated_Code/PE_Timer.obj" "../Generated_Code/PE_Timer.c"'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PE_Timer.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
Object file: Generated_Code/PE_Timer.obj, format ELF/DWARF 2.0
Code Size: 567
Global objects: 10
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PE_Timer.args" -ObjN="Generated_Code/PE_Timer.obj" "../Generated_Code/PE_Timer.c" -Lm="Generated_Code/PE_Timer.d" -LmCfg=xilmou
../Generated_Code/PE_Timer.c
Command Line: '-ArgFile"Generated_Code/PE_Timer.args" -ObjN="Generated_Code/PE_Timer.obj" "../Generated_Code/PE_Timer.c" -Lm="Generated_Code/PE_Timer.d" -LmCfg=xilmou'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PE_Timer.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
Option -Lm Update: Create new dependency file
Option -Lm: Adding make info to 'Generated_Code/PE_Timer.d'
Object file: Generated_Code/PE_Timer.obj, format ELF/DWARF 2.0
Code Size: 567
Global objects: 10
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/PE_Timer.c'
' '
'Building file: ../Generated_Code/PwrCtl.c'
'Invoking: HCS08 Compiler'
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PwrCtl.args" -ObjN="Generated_Code/PwrCtl.obj" "../Generated_Code/PwrCtl.c"
../Generated_Code/PwrCtl.c
Command Line: '-ArgFile"Generated_Code/PwrCtl.args" -ObjN="Generated_Code/PwrCtl.obj" "../Generated_Code/PwrCtl.c"'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PwrCtl.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
Object file: Generated_Code/PwrCtl.obj, format ELF/DWARF 2.0
Code Size: 13
Global objects: 2
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PwrCtl.args" -ObjN="Generated_Code/PwrCtl.obj" "../Generated_Code/PwrCtl.c" -Lm="Generated_Code/PwrCtl.d" -LmCfg=xilmou
../Generated_Code/PwrCtl.c
Command Line: '-ArgFile"Generated_Code/PwrCtl.args" -ObjN="Generated_Code/PwrCtl.obj" "../Generated_Code/PwrCtl.c" -Lm="Generated_Code/PwrCtl.d" -LmCfg=xilmou'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PwrCtl.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
Option -Lm Update: Create new dependency file
Option -Lm: Adding make info to 'Generated_Code/PwrCtl.d'
Object file: Generated_Code/PwrCtl.obj, format ELF/DWARF 2.0
Code Size: 13
Global objects: 2
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/PwrCtl.c'
' '
'Building file: ../Generated_Code/PwrSwitchMonitor.c'
'Invoking: HCS08 Compiler'
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PwrSwitchMonitor.args" -ObjN="Generated_Code/PwrSwitchMonitor.obj" "../Generated_Code/PwrSwitchMonitor.c"
../Generated_Code/PwrSwitchMonitor.c
Command Line: '-ArgFile"Generated_Code/PwrSwitchMonitor.args" -ObjN="Generated_Code/PwrSwitchMonitor.obj" "../Generated_Code/PwrSwitchMonitor.c"'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PwrSwitchMonitor.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
Object file: Generated_Code/PwrSwitchMonitor.obj, format ELF/DWARF 2.0
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/PwrSwitchMonitor.args" -ObjN="Generated_Code/PwrSwitchMonitor.obj" "../Generated_Code/PwrSwitchMonitor.c" -Lm="Generated_Code/PwrSwitchMonitor.d" -LmCfg=xilmou
../Generated_Code/PwrSwitchMonitor.c
Command Line: '-ArgFile"Generated_Code/PwrSwitchMonitor.args" -ObjN="Generated_Code/PwrSwitchMonitor.obj" "../Generated_Code/PwrSwitchMonitor.c" -Lm="Generated_Code/PwrSwitchMonitor.d" -LmCfg=xilmou'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\PwrSwitchMonitor.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
Option -Lm Update: Create new dependency file
Option -Lm: Adding make info to 'Generated_Code/PwrSwitchMonitor.d'
Object file: Generated_Code/PwrSwitchMonitor.obj, format ELF/DWARF 2.0
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/PwrSwitchMonitor.c'
' '
'Building file: ../Generated_Code/RS232.c'
'Invoking: HCS08 Compiler'
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/RS232.args" -ObjN="Generated_Code/RS232.obj" "../Generated_Code/RS232.c"
../Generated_Code/RS232.c
Command Line: '-ArgFile"Generated_Code/RS232.args" -ObjN="Generated_Code/RS232.obj" "../Generated_Code/RS232.c"'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\RS232.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\RS232.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Sources\Events.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\BRIDGE_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyCol_In.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyLed.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyRowStrobe.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_CTL.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_Light.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCDDATA.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Led.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Tmr100hz.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\USB.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_PROGn.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_RESETn.h"
Object file: Generated_Code/RS232.obj, format ELF/DWARF 2.0
Code Size: 548
Global objects: 29, Data Size (RAM): 135
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/RS232.args" -ObjN="Generated_Code/RS232.obj" "../Generated_Code/RS232.c" -Lm="Generated_Code/RS232.d" -LmCfg=xilmou
../Generated_Code/RS232.c
Command Line: '-ArgFile"Generated_Code/RS232.args" -ObjN="Generated_Code/RS232.obj" "../Generated_Code/RS232.c" -Lm="Generated_Code/RS232.d" -LmCfg=xilmou'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\RS232.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\RS232.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Sources\Events.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\BRIDGE_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyCol_In.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyLed.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyRowStrobe.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_CTL.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_Light.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCDDATA.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Led.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Tmr100hz.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\USB.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_PROGn.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_RESETn.h"
Option -Lm Update: Create new dependency file
Option -Lm: Adding make info to 'Generated_Code/RS232.d'
Object file: Generated_Code/RS232.obj, format ELF/DWARF 2.0
Code Size: 548
Global objects: 29, Data Size (RAM): 135
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/RS232.c'
' '
'Building file: ../Generated_Code/Tmr100hz.c'
'Invoking: HCS08 Compiler'
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/Tmr100hz.args" -ObjN="Generated_Code/Tmr100hz.obj" "../Generated_Code/Tmr100hz.c"
../Generated_Code/Tmr100hz.c
Command Line: '-ArgFile"Generated_Code/Tmr100hz.args" -ObjN="Generated_Code/Tmr100hz.obj" "../Generated_Code/Tmr100hz.c"'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\Tmr100hz.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Sources\Events.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\BRIDGE_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyCol_In.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyLed.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyRowStrobe.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_CTL.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_Light.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCDDATA.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Led.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\RS232.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Tmr100hz.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\USB.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_PROGn.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_RESETn.h"
Object file: Generated_Code/Tmr100hz.obj, format ELF/DWARF 2.0
Code Size: 80
Global objects: 12, Data Size (RAM): 1
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
"C:\Freescale\CW MCU v10.0\eclipse\../MCU/prog/chc08" -ArgFile"Generated_Code/Tmr100hz.args" -ObjN="Generated_Code/Tmr100hz.obj" "../Generated_Code/Tmr100hz.c" -Lm="Generated_Code/Tmr100hz.d" -LmCfg=xilmou
../Generated_Code/Tmr100hz.c
Command Line: '-ArgFile"Generated_Code/Tmr100hz.args" -ObjN="Generated_Code/Tmr100hz.obj" "../Generated_Code/Tmr100hz.c" -Lm="Generated_Code/Tmr100hz.d" -LmCfg=xilmou'
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Project_Headers\../Generated_Code\Tmr100hz.c"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Sources\Events.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Types.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Error.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Const.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\IO_Map.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PE_Timer.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\BRIDGE_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Cpu.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyCol_In.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyLed.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\KeyRowStrobe.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_CTL.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_EN.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCD_Light.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\LCDDATA.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Led.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrCtl.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\PwrSwitchMonitor.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\RS232.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\Tmr100hz.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\USB.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_PROGn.h"
"C:/Users/Jake/CodeWarrior Workspace/SLP_2/Generated_Code\VINC_RESETn.h"
Option -Lm Update: Create new dependency file
Option -Lm: Adding make info to 'Generated_Code/Tmr100hz.d'
Object file: Generated_Code/Tmr100hz.obj, format ELF/DWARF 2.0
Code Size: 80
Global objects: 12, Data Size (RAM): 1
HC08 Compiler: *** 0 error(s), 0 warning(s), 0 information message(s) ***
HC08 Compiler: *** Processing ok ***
'Finished building: ../Generated_Code/Tmr100hz.c'
' '

0 项奖励
回复
3,189 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

I don't see that error in your log file extract you have posted? Maybe the text go cut?

 

BK

0 项奖励
回复
3,189 次查看
BlackNight
NXP Employee
NXP Employee

as a suggestion: you can copy-paste the console output to a text file and attach that file. That way you do not run into the post size limitation.

 

BK

0 项奖励
回复
3,189 次查看
JakeP
Contributor I

Looks like part 2 didn't make it, sorry...  Attached is a text file with the whole console output for a clean+build.

 

Thanks

0 项奖励
回复
3,189 次查看
JakeP
Contributor I

Since the ProcessorExpert.obj and Events.obj files are present in the project but the compiler is complaining that it can't read them, I'm guessing they got corrupted somewhere along the way.  If I delete the files from the project and then run a "generate processor expert code" command would that regenerate the files?  If not how would I regenerate the files?

 

Thanks

0 项奖励
回复
3,189 次查看
CompilerGuru
NXP Employee
NXP Employee

They should be deleted when you do a clean, are they not regenerated? I would expect that to happen. Check the file dates for example.

The logs did not show those files to be generated, but apears to be a partial log. For a full one you might have to increase the size of the console.

 

I don't think the obj files are corrupted.

I read

ERROR L1818: Symbol 23 - error duplicated in ProcessorExpert.obj and Events.obj

to mean that there was a symbol called error defined in both ProcessorExpert.c and in Events.c.

I guess the error symbol is the 23'th in the ELF symbol table in ProcessorExpert.obj, but that's just a unimportant detail.

 

The second error message

ERROR L1301: Cannot open file ./Sources/ProcessorExpert.obj

just means something failed whiile looking at the content of ProcessorExpert.obj, it does not mean that object file got corrupted.

 

So I would look through the source code and check if there is any symbol called error defined in those files (or in any header included by them).

 

Daniel

 

 

0 项奖励
回复
3,192 次查看
CompilerGuru
NXP Employee
NXP Employee

When adding this line to main.c and a newly created file s.c

> int defined_twice=2;

 

I get these errors in the problems view:

 

Cannot open file ./Sources/s.obj s08 line 0 C/C++ Problemmake: *** [s08.abs] Error 1 s08 line 0 C/C++ ProblemSymbol 14 - defined_twice duplicated in s.obj and main.obj s08 line 0 C/C++ Problem

 

The problems view sorts them by the description, which is a bit unfortunate as the last one actually caused the two other messages. Also the "Cannot open file" is a bit misleading, as it can open it, the linker just does not like the content.

 

Just added this to show that the error in the original report just is a variable or function name and not part of the message.

 

Daniel

 

0 项奖励
回复
3,191 次查看
JakeP
Contributor I

Yep you're right, I did have a variable named "error" that was declared in both ProcessorExpert.c and Events.c.  That's obviously a bad variable name because I thought it was a part of the console output like you said.  I corrected the declarations and now the project builds correctly.

 

Thank you for all the help!

 

-Jake

0 项奖励
回复