CW10.6 will not create a s-record flash image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.6 will not create a s-record flash image

Jump to solution
1,587 Views
pbanta
Contributor IV

I have a one project where CW10.6 will not produce a flash image.  In C/C++ Build/Settings/Additional Tools I have "Create Flash Image" and "Print Size" both checked.  Neither one of those two tools is invoked at the end of the link stage.

 

I have other CW10.6 projects where I have both tools checked and I get a size and hex (s-record) file.

 

I saw another posting about a similar issue in KDS where the author disabled parallel compile option and got his post build script running.  I tried disabling the parallel build but it didn't help.

 

Any ideas?

Labels (1)
1 Solution
1,423 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
1,424 Views
BlackNight
NXP Employee
NXP Employee

Have you set 'per file' options?

See Traps and Pitfalls: No Hex/Bin/S19 File Created with GNU? | MCU on Eclipse

I hope this helps,

Erich

0 Kudos
Reply
1,423 Views
pbanta
Contributor IV

Thank you, Erich! 

There were four such files in the project that had per file permissions set.

0 Kudos
Reply