Hello,
We have used in the past the older standalone 56800E Flash Programmer app that came with the CW8.x tools. We have upgraded our PC to a WIN7 Pro machine now we are trying to use newer tools for production programming of our products. We have installed CW10.6.4 and setup the FLASH Programmer as a Task.
I am able to connect to the USB Tap and everything seems to start OK:
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Motorola S-Record Format.
Auto-detection is successful.
File is of type Motorola S-Record Format.
Erasing ..............
Error: Erase Command Failed. Protect violation error.
Error: Erase Command Failed. Protect violation error.
fl::target -lc "LC for Simple Flash"
fl::target -b 0x2fc00 0x400
fl::target -v off -l off
cmdwin::fl::device -d "MC56F8323_P_FLASH" -o "68kx16x1" -a 0x0 0x20fff
cmdwin::fl::protect all off
Beginning Operation ...
-------------------------
Performing target initialization ...
Flash Operation.
Unprotecting .............
Unprotect Command Succeeded.
cmdwin::fl::erase all
-------------------------
Erasing ..........
Error: Erase Command Failed. Protect violation error.
Error: Erase Command Failed. Protect violation error.
My Setups look like this:
So as you can see it appears everything is setup correctly and I have tried multiple target boards. Any ideas on how to correct the "Error: Erase Command Failed. Protect violation error." would be great.
Thanks,
Dave
解決済! 解決策の投稿を見る。
Hi,
CodeWarrior v10.6.4 has problem in programming 56F8323 with USBTAP, user needs to manually update the .tcl and xml file in CodeWarrior and project folder. For details, please refer to:
https://community.freescale.com/docs/DOC-105548
In addition, 56800E Flash Programmer v1.2 also works on Windows 7-64bit, please copy the CCS folder in CW10.6.4 and use it to replace the one under 56800E Flash Programmer v1.2. For details, pleases refer to:
https://community.freescale.com/docs/DOC-102607
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
CodeWarrior v10.6.4 has problem in programming 56F8323 with USBTAP, user needs to manually update the .tcl and xml file in CodeWarrior and project folder. For details, please refer to:
https://community.freescale.com/docs/DOC-105548
In addition, 56800E Flash Programmer v1.2 also works on Windows 7-64bit, please copy the CCS folder in CW10.6.4 and use it to replace the one under 56800E Flash Programmer v1.2. For details, pleases refer to:
https://community.freescale.com/docs/DOC-102607
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------