CW10.5 crash and sluggish

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW10.5 crash and sluggish

Jump to solution
1,875 Views
DavidS
NXP Employee
NXP Employee

Hello,

Has anyone any suggestions on below customer issue?

Regards,

David

 

Even more seriously, beginning last week, the IDE quickly becomes sluggish to the point of being unusable, eventually crashing with an error message about "Java heap space". It's so repeatable that all I have to do is open a workspace and do nothing else - within 5 minutes it will crash - sooner, if I try to do anything with the project.

 

I've reinstalled codewarrior. I've reinstalled Java. I even reformmated my hard drive and installed a fresh copy of Windows with nothing else installed on the system, except Office, Java and CodeWarrior, and still it happens.

 

Have you seen anything like this?

 

I'm running Windows7 on a Dell laptop.

Labels (1)
0 Kudos
Reply
1 Solution
1,621 Views
matthewkendall
Contributor V
0 Kudos
Reply
2 Replies
1,622 Views
matthewkendall
Contributor V
0 Kudos
Reply
1,621 Views
DavidS
NXP Employee
NXP Employee

Thank you Matthew. Will have my customer give this a try.

Regards,

David

0 Kudos
Reply