CW v10 not working with PE DEMOJM board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW v10 not working with PE DEMOJM board

ソリューションへジャンプ
1,590件の閲覧回数
donw
Contributor IV

Hi all

I am trying to get CW v10 to download code to the P&E DemoJM board.

(Win7, 64 bit )

The board works OK under CW 6.1. 

The 'P&E Connection Assistant' in the debugger shows that the board is connected 'USB-ML12: DEMOJM on USB1'

but it just says 'an error occurred', retry when trying to download code.

the error message 'HC GDI Protocol Adapter:  Can't connect . The debugger cannot connect to the PE device.' when quitting the connection.

The first time I connected there was a (fast) code update of the multilink code in the board.

 

the HCS08 debugger is 10.0.0.FSL_b2619

 

Has anyone had CW working with this board? (or is there a bug as in CW v6.3 which does the same thing)

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
817件の閲覧回数
HCatalin
NXP Employee
NXP Employee

If the update dialog popup it means that your P&E debug probe was detected.

Before launching the debug session I suggest you open the Launch configuration dialog (LCD), go to the Connection tab and try to detect the P&E probe.

I'm sure why is not working since the probe was detected. In this case the debug session log can help. You can enable the logger from the LCD in the Conenction tab.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
818件の閲覧回数
HCatalin
NXP Employee
NXP Employee

If the update dialog popup it means that your P&E debug probe was detected.

Before launching the debug session I suggest you open the Launch configuration dialog (LCD), go to the Connection tab and try to detect the P&E probe.

I'm sure why is not working since the probe was detected. In this case the debug session log can help. You can enable the logger from the LCD in the Conenction tab.

 

0 件の賞賛
返信