CW HC(s)12 v3.1 - Dead P&E Multilink Rev. B - What to do?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW HC(s)12 v3.1 - Dead P&E Multilink Rev. B - What to do?

ソリューションへジャンプ
1,692件の閲覧回数
Shortbus
Contributor I
Hello.
 
I zapped my Multilink Rev. B!  From what I can tell, P&E isn't making Rev. B BDM pods anymore, yet that's the latest rev. that our CodeWarrior HC(s)12 V3.1 installs will work with.
 
Considering the fact that money is tight, where should I proceed from here? 
 
Is there still a source of Rev. B multilinks?  We have two CW 3.1 installs here that could potentially be unusable if we can't debug anymore. 
 
Is there a way I can use a Rev C BDM with my CW v3.1?    If not, is there an affordable(!!) upgrade path to a later version of codewarrior that works with rev. C pods?
 
Thanks in advance,
 
Craig Iannello
Embedded Sys.
Sun Nuclear Corp.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
656件の閲覧回数
Lundin
Senior Contributor IV
I have been using P&E Cyclone Pro rev C with CW3.1 since they released rev C, so both multilinks and Cyclones of rev C should work without problems. What made you think it wouldn't work?

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
657件の閲覧回数
Lundin
Senior Contributor IV
I have been using P&E Cyclone Pro rev C with CW3.1 since they released rev C, so both multilinks and Cyclones of rev C should work without problems. What made you think it wouldn't work?
0 件の賞賛
返信