CW 6.0 Visualization Tool querry.??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 6.0 Visualization Tool querry.??

Jump to solution
1,674 Views
Destiny
Contributor I
Dear all
  
   Currently I am reading some values from the Microcontroller. So for easy to read option I am using the Visualisation tool
   In visualisation tool I am using the Value as text option, so the values which are displaced are rounded ones, but instead I would be glad to have values with digits after the decimal points.
   So is there any way to get complete value in Visualisation tools,  instead of rounding off ones???

thanks in advanced

Regards
Destiny
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
904 Views
CrasyCat
Specialist III
Hello
 
The visualization tool is not able to display a floating point value.
 
It displays the hexadecimal encoding of the variable (or the decimal representation of the 4-byte value read as a long).
 
You may want to submit a feature request if you need to get that supported in the visualization tool.

Click here to submit a service request.

 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
905 Views
CrasyCat
Specialist III
Hello
 
The visualization tool is not able to display a floating point value.
 
It displays the hexadecimal encoding of the variable (or the decimal representation of the 4-byte value read as a long).
 
You may want to submit a feature request if you need to get that supported in the visualization tool.

Click here to submit a service request.

 
CrasyCat
0 Kudos
Reply