CW 10 beta, where is HC08?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10 beta, where is HC08?

3,627 Views
jarin
Contributor I

Hello all,

 

I installed CW10.0 and after years of use of CW products I'm really ugly disappointed. Except of the fact it is based o Eclipse, what I will not discuss here, I noticed missing support for HC08 MCUs.

What can I do to support old (5 years!) devices based around HC08 chips? HC08 is not legacy MCU family and its members are still marked as "Active", so I expect it to be supported.

 

Thanks all,

 

J.

Labels (1)
Tags (1)
0 Kudos
Reply
8 Replies

2,148 Views
GR8geek
Contributor II

CodeWarrior 10.0 will not support HC08 parts, according to CW team pitch at FTF Americas (June, 2010).

0 Kudos
Reply

2,148 Views
admin
Specialist II

Have you ever really used CW10.0?

Check FSL link for CW 10.0, HCS08 is supported by CW10.0

www.freescale.com/cwmcu10

Here is the list of device support:

  • HCS08: AC, AW, DE, DN, DV, DZ, EL, EN, FL, GB, GT, JE, JM, JR, JS, LC, LG, LH, LL, MM, MP, QA, QB, QD, QE, QG, RC, RD, RE, RG, SC, SE, SG, SH, SL, SV, MC1321X, MPXY
  • RS08: KA, KB, LA, LE
  • V1 ColdFire: AC, AG, CN, EM, JE, JM, MM, QE
  • V2 ColdFire: MCF520x, MCF521x, MCF523x, MCF524x, MCF525x, MCF527x, MCF528x, MCF521x0, MCF5221x, MCF5222x, MCF5223x, MCF5225x, MCF5227x
  • V3 ColdFire: MCF530x, MCF532x, MCF537x, MCF5301x
  • V4 ColdFire: MCF540x, MCF5445x
  • V4e ColdFire: MCF547x, MCF548x
0 Kudos
Reply

2,148 Views
peg
Senior Contributor IV

Yes!

 

HC08 not included!

 

HCS08 (S08) is not the same thing as HC08. Completely different cores.

 

0 Kudos
Reply

2,148 Views
stanish
NXP Employee
NXP Employee

Hello,

 

As far as I know HC08 should be supported by the CodeWarrior classic (non-Eclipse).

The latest version is v6.3 available here:

http://cache.freescale.com/lgfiles/devsuites/HC08/CW_MCU_V6_3_SE.exe

 

Stanish

0 Kudos
Reply

2,148 Views
jarin
Contributor I

Thanks for responses.

 

So, for HCS08 there is CW10.0 (Eclipse based) and CW6.3 (non-Eclipse).

For HC08 there is CW6.3 only.

 

Will freescale update non-Eclipse based CW versions in future, or this (CW6.3) is last non-Eclipse version and further developement will be moved to Eclipse based CW?

0 Kudos
Reply

2,148 Views
J2MEJediMaster
Specialist I

I cannot comment on future product directions. However, what I would suggest is that you file a service request on the lack of HC08 support in MCU v10. That way your request gets logged and the engineering team is made aware of it. I cannot guarantee that the feature will be added, but getting it in front of the engineers is a good start. Click here to file a service request.

 

---Tom

0 Kudos
Reply

2,148 Views
jarin
Contributor I

Thank you,

 

I placed request as you suggested.

Hopefully HC08 is not definitively lost.

0 Kudos
Reply

2,148 Views
Lundin
Senior Contributor IV

I thought the latest CW for HC80 was version 6.2?

 

0 Kudos
Reply