CW 10.8 - Gigabit TAP: "CCS: Connection refused"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.8 - Gigabit TAP: "CCS: Connection refused"

Jump to solution
2,166 Views
rainerhaseneder
Contributor II

Hello,

 

I try to connect from Windows 7 PC with CW (CodeWarrior Development Studio For StarCore) 10.8

via a Gigabit TAP to my SoC (B4680) by launching a group launcher and get following error message (IP-connection PC<->TAP is OK):

 

   Error launching (my-launcher-filename)

     CCSProtocolPlugin : CCS: Connection refused

 

Please check out also the attached screenshots.

Does anyone have an idea ?

 

Thank you.

 

Rainer Haseneder

 

PS

 

Regarding versions and CCS output:

 

- My Gigabit TAP (version unknown)

 

- in CCS I see:

(bin) 25 % show version

Received  CMD_SERVER_VERSION

command done - Ok

CCS Windows Release Build 400p0

CodeWarrior Connection Server version {4.13}

(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED

(bin) 26 %

 

- CCS help info:

About CCS

CCS Windows Release Build 400p0

CodeWarrior Connection Server version {4.13}

(C) Copyright 2003-2010 Freescale Semiconductor, Inc. ALL RIGHTS RESERVED

 

cw_support@freescale.com 

http://www.freescale.com/codewarrior

 

- The CCS protocol shows:

CCSAPI connection #1 accepted from DESTGN0H464066.emea.lucent.com at Wed Dec 02 12:22:15 2015

Received  CMD_CHECK_MIN_VERSION

command done - Ok

Received  CMD_GET_CONNECTION_COUNT

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received  CMD_AVAILABLE_CONNECTIONS

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

command done - Ok

Received an unknown command 140

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

Received  CMD_GET_REMOTE_USER

command done - Ok

Received  CMD_CC_VERSION

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

Received  CMD_CONFIG_CHAIN. count = 0

Received  CMD_CC_VERSION

nhti command done - Ok

nhti command done - Ok

nhti command done - Connection refused

CCSAPI connection #1 from DESTGN0H464066.emea.lucent.com closed at Wed Dec 02 12:22:16 2015

(bin) 24 %

Labels (1)
0 Kudos
1 Solution
1,595 Views
lunminliang
NXP Employee
NXP Employee

Hello Rainer Haseneder,

Have you configured the connection type to be gigabit tap? What probe tip do you use?

You may also try to update the firmware.

Regards

View solution in original post

0 Kudos
3 Replies
1,594 Views
mukunkong
Contributor I

when i used codewarrior for QorIQ,I intened to connect CodeWarrior TAP wtih net,i use port 41475, happended same problem to you,problem which you find whether ok or not?

0 Kudos
1,596 Views
lunminliang
NXP Employee
NXP Employee

Hello Rainer Haseneder,

Have you configured the connection type to be gigabit tap? What probe tip do you use?

You may also try to update the firmware.

Regards

0 Kudos
1,595 Views
rainerhaseneder
Contributor II

Hello,

thank you for the answer.

I am using a flat ribbon cable with an Aurora connector.

How do I check the FW version ? Is there a CCS command ?

BR
Rainer

0 Kudos