CW 10.6 Terminal Serial Com Port Conncetion Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10.6 Terminal Serial Com Port Conncetion Error

Jump to solution
1,777 Views
projektecarus
Contributor II

Hi,

I'm trying to use the Terminal via the virtual Serial Com Port for debugging my application on a k60f120m Kinetis Tower. But every time I try to establish a connection to the Port, I'm getting conncetion error

68307_68307.PNGerror.PNG

although there's no other application using the COM Port.

Sometimes the message changes to "there is no COM.. Port"

I managed to establish a conncetion once by chance. But after I closed the conncetion, I couldn't establish it again.

Any suggestions why it isn't working?

Labels (1)
0 Kudos
Reply
1 Solution
1,522 Views
trytohelp
NXP Employee
NXP Employee

Hi,

What is saying the Device Manager for the Com port ?

This is listed under Ports (COM & LPT)

Do you use physical COM or a cable USB->COM

Did you tried to use another port (other USB)?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,522 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please check the COM port on the PC Device Manager ,

check whether is COM4 .

And please be sure on your PC , whether it already open one serial terminal , if yes , please first close it .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,522 Views
projektecarus
Contributor II

COM port is corret and there is no other application using it.

0 Kudos
Reply
1,523 Views
trytohelp
NXP Employee
NXP Employee

Hi,

What is saying the Device Manager for the Com port ?

This is listed under Ports (COM & LPT)

Do you use physical COM or a cable USB->COM

Did you tried to use another port (other USB)?

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply