CW 10.4 editor & include browser display problem for PXS30_Tower project. Operator error?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 10.4 editor & include browser display problem for PXS30_Tower project. Operator error?

1,900 次查看
paul_murray
Contributor II

Is anyone else seeing this issue?

 

    The PXS30_Tower project defines two Project Configuration options:

    PXS3020_INTERNAL_RAM and PXS3020_INTERNAL_FLASH. The Prefix subdirectory

    has an include file for each.

 

    PXS3020_INT_FLASH_VLE_DPM.prefix contains '#define ROM_VERSION 1',

    PXS3020_INT_RAM_VLE_DPM.prefix has no define for ROM_VERSION.

    So...

 

    If I select PXS3020_INTERNAL_RAM as my Project Configuration and open

    PRC1_Sources/_start_p1.c and look at line 110, I see a conditional

    block grayed-out as expected, because ROM_VERSION is not defined by

    PXS3020_INT_RAM_VLE_DPM.prefix. So good so far.

 

    However, if I select PXS3020_INTERNAL_FLASH and look at line 110 of

    _start_p1.c, the preprocessor block remains grayed-out.

    If I open an 'Include Browser' window and drop _start_p1.c into it,

    the first file listed is PXS3020_INT_RAM_VLE_DPM.prefix. This is true

    for either Project_Configuration.

 

    NB: This is simply a viewing problem; the builds include the correct

    prefix files and generate the correct code. There is probably a simple

    fix?

 

 

 

标签 (1)
0 项奖励
回复
2 回复数

1,796 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

it looks like a CW IDE problem. can you please upload the demo project here, so that we can reproduce and confirm it?

0 项奖励
回复

1,796 次查看
paul_murray
Contributor II

Thanks for your response.  It would be interesting to see if you get (as I suspect) the same behavior with the vanilla software packaged with cw10.4.

I'll be glad to upload my (slightly modified) demo, but can't find upload packaging instructions.  I know I've seen them, but can't find then this morning.  Any suggestions?

0 项奖励
回复