CW 10.3 and Freescale S09AW32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.3 and Freescale S09AW32

704件の閲覧回数
chinniwhites
Contributor II

I am trying to create a bareboard project in CW 10.3 and having no success.  As soon as I finish the add project wizard, its like nothing even happened; no folder in workspace, nothing.  The micro is a mcs09aw32.  I think it has something to do with trying to use Processor Expert.  If I keep default setting the same, it will create the project.  If I choose any of the rapid development tools (device initialization or processor expert, it doesnt create the project.  Whats up?

ラベル(1)
0 件の賞賛
返信
0 返答(返信)