Good day Erich,
Thank you for your response and kudos to you on your site! There is a lot of valuable information there!
As for this CW issue... Indeed, I understand this, but I am amazed that an application would feel the need to permanently delete files itself as opposed to deleting via the O/S. I say this as if the latter is done, then one could recover the files from the Recycle or Trash bin... Given the seriousness of doing a whole sub-folder deletion, I (if I was the CW application programmer) would have added a dialog box with a "Are you sure?" question. In my case a simple bumping of the mouse against a keyboard deleted all of the files within a project sub folder that were all unrecoverable except for two files. Thankfully I backup often and so it took a while to piece each file, etc in order to get back to where I was.
Adding to all this I had another major issue with CW where I made one small change to my application and I was unable to compile (I had 0 errors and then one change resulted in 906 errors... removed the change and I was still unable to compile), debug, etc. In this case a previous day's backup would not restore the system. I had to go back to another backup, re-import the project, and then restore the newer files piece-meal. Overall my experience with CW 10.x has been poor. CW Classic, on the other hand, was/is significantly better and so I guess that was my standard...
Anyway, thank you for your post and your great site!
Cheers,
Sam