CW 10.2 App fails to compile after conversion to CW 10.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10.2 App fails to compile after conversion to CW 10.4

870件の閲覧回数
huguesleger
Contributor I

I imported a 10.2 project into CW 10.4; now the application will not compile. The application is set up to create an s-record as output. I found out unless I specify and extension for the build artifact (Propeties->C/C++ Build->Settings) in the Build Articat tab, or add a dot (.) to the Artifact name (e.g. console.flash), the project will not compile.  When in Properties->Settings->ColdFire Linker->Output window, the Generate S-Record File box is checked, the artifact extension must remain blank as the s19 extensition will automatically be added to the file name.  Has anyone else run into this problem with CW 10.4? Does anyone know if this issue is being addressed in CW 10.4.2?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

773件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

I just got information from DevTech that we can not reproduced the problem with CW10.5 now.

CW10.5 will get released on the end of this month. It will be posted at this link then:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&fpsp=1&tab=Design_Tools_Tab

0 件の賞賛
返信