CW 10.2 App fails to compile after conversion to CW 10.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW 10.2 App fails to compile after conversion to CW 10.4

849 次查看
huguesleger
Contributor I

I imported a 10.2 project into CW 10.4; now the application will not compile. The application is set up to create an s-record as output. I found out unless I specify and extension for the build artifact (Propeties->C/C++ Build->Settings) in the Build Articat tab, or add a dot (.) to the Artifact name (e.g. console.flash), the project will not compile.  When in Properties->Settings->ColdFire Linker->Output window, the Generate S-Record File box is checked, the artifact extension must remain blank as the s19 extensition will automatically be added to the file name.  Has anyone else run into this problem with CW 10.4? Does anyone know if this issue is being addressed in CW 10.4.2?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

752 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I just got information from DevTech that we can not reproduced the problem with CW10.5 now.

CW10.5 will get released on the end of this month. It will be posted at this link then:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&fpsp=1&tab=Design_Tools_Tab

0 项奖励
回复