Processor Expert error says my external crystal is out of range. The MCU Specification Manual says I can go as high as 40Mhz with an external crystal. The error says that the limit is 8Mhz however in the error message it states the range is 0-40Mhz butr it only gives me an option up to 8Mhz. I want to use a 22.1184Mhz crystal oscillator. How can I make this work?
解決済! 解決策の投稿を見る。
Hello,
for more detals about settings of ICG module please see “Table A-11. ICG Frequency Specifications“ table in MC9S08AC16 datasheet (in Apendix A). I have also checked behaviour of AC16 CPU component and I think that it behaves according to this table and the PE documentation. Attached screen-shot shows how to set the CPU component to run from 22.1184 MHz oscillator.
best regards
Vojtech Filip
Processor Expert Support Team
Hi Spooky,
The difference in specs has to do with the difference between a crystal and an oscillator. The first sentence of your post states that you are using a crystal, but later you state that you are using an oscillator.
The AC16's internal oscillator circuitry can only drive a crystal up to 8 mHz. But the AC16 can accept an external clock up to 40 mHz. So an external oscillator of 22.1184 mHz should work.
What I can't help you with is how to tell Processor Expert whether you have a crystal or an external clock. That seems to be a separate problem.
Hello,
for more detals about settings of ICG module please see “Table A-11. ICG Frequency Specifications“ table in MC9S08AC16 datasheet (in Apendix A). I have also checked behaviour of AC16 CPU component and I think that it behaves according to this table and the PE documentation. Attached screen-shot shows how to set the CPU component to run from 22.1184 MHz oscillator.
best regards
Vojtech Filip
Processor Expert Support Team