CPU MC9S08AC16 clock out of range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CPU MC9S08AC16 clock out of range

跳至解决方案
1,660 次查看
Spookydude
Contributor III

Processor Expert error says my external crystal is out of range.  The MCU Specification Manual says I can go as high as 40Mhz with an external crystal.  The error says that the limit is 8Mhz however in the error message it states the range is 0-40Mhz butr it only gives me an option up to 8Mhz.  I want to use a 22.1184Mhz crystal oscillator.  How can I make this work?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,197 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

for more detals about settings of ICG module please see “Table A-11. ICG Frequency Specifications“ table in MC9S08AC16 datasheet (in Apendix A). I have also checked behaviour of AC16 CPU component and I think that it behaves according to this table and the PE documentation. Attached screen-shot shows how to set the CPU component to run from 22.1184 MHz oscillator.

 

best regards
Vojtech Filip
Processor Expert Support Team

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,197 次查看
rocco
Senior Contributor II

Hi Spooky,

 

The difference in specs has to do with the difference between a crystal and an oscillator. The first sentence of your post states that you are using a crystal, but later you state that you are using an oscillator.

 

The AC16's internal oscillator circuitry can only drive a crystal up to 8 mHz. But the AC16 can accept an external clock up to 40 mHz. So an external oscillator of 22.1184 mHz should work.

 

What I can't help you with is how to tell Processor Expert whether you have a crystal or an external clock. That seems to be a separate problem.

0 项奖励
回复
1,198 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

for more detals about settings of ICG module please see “Table A-11. ICG Frequency Specifications“ table in MC9S08AC16 datasheet (in Apendix A). I have also checked behaviour of AC16 CPU component and I think that it behaves according to this table and the PE documentation. Attached screen-shot shows how to set the CPU component to run from 22.1184 MHz oscillator.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复