I am using Code Warrior version 10.3 evaluation version.
We don't have a target board now.
So, I am trying to create a Simulator project.
For this I have selected P4080 processor.
I didn't modify any code after creating the project.
(There were some printf's in the main.c of Sources folder).
So, I just compiled the code. It happened successfully. And now when I tried to run, an error occured.
The issues which I faced are attached here as screenshots (as P4080_Simulator1 and P4080_Simulator2).
The procedure which I followed for creating, building and running a project is attached below as P4080_CW_SShots.doc.