CAU_LDD unsupported in upgrade from 10.6 to 10.6.4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAU_LDD unsupported in upgrade from 10.6 to 10.6.4?

922 Views
panometric
Contributor I

Importing a project from 10.6, but it will not build on 10.6.4 because Processor Expert will not generate code for the crypto module. The CPU is MCF51QM128VHS. The help for the module shows fine, and the files appear to be installed.

But the processor expert window says that CAU_LDD  module is not supported in this version of Processor Expert. See attached.  How can this be fixed? 

Tags (1)
0 Kudos
Reply
1 Reply

735 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

CAU_LDD component is deprecated and not integrated in the new version.

Our recommendation is

Crypto Acceleration Unit: CAU and mmCAU software library|NXP 

Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply