Build of Codewarrior 10.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build of Codewarrior 10.3

Jump to solution
1,235 Views
Microfelix
Contributor IV

hello

Using CodeWarrior 10.3 for kinetis K70.

I installed CodeWarrior both on the PC and I have the fixed version 10.3 build 131xxx, while on the laptop I have version 10.3 build 121xxx.

Because the lower build does not update like the desktop computer?

 

 

thanks

 

Maurizio

 

Labels (1)
0 Kudos
Reply
1 Solution
1,075 Views
BlackNight
NXP Employee
NXP Employee

Hi Maurizio,

b131xxx was on the web/availble only for a short period of time (a few days I think), until it got pulled off.

The problem is an installer issue, see

Recent upgrade breaks project

So you might have been lucky (or unlucky) that you installed the update.

The update works fine if

a) you are not doing debugging during the update, and

b) you have not started a debug session before the update

Otherwise the installation might not work correctly, as seen in the previous report.

Because it is such a high risk, Freescale has pulled off the update, and will release it again once the problem is fixed.

View solution in original post

0 Kudos
Reply
2 Replies
1,076 Views
BlackNight
NXP Employee
NXP Employee

Hi Maurizio,

b131xxx was on the web/availble only for a short period of time (a few days I think), until it got pulled off.

The problem is an installer issue, see

Recent upgrade breaks project

So you might have been lucky (or unlucky) that you installed the update.

The update works fine if

a) you are not doing debugging during the update, and

b) you have not started a debug session before the update

Otherwise the installation might not work correctly, as seen in the previous report.

Because it is such a high risk, Freescale has pulled off the update, and will release it again once the problem is fixed.

0 Kudos
Reply
1,075 Views
Microfelix
Contributor IV

Thanks

0 Kudos
Reply