Bug fixes in CodeWarrior releases

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug fixes in CodeWarrior releases

ソリューションへジャンプ
2,334件の閲覧回数
June
Contributor I

Hi,

I'm reviewing the release notes between CodeWarrior v10.4 versus v10.5. There are some known issues noted in v10.4 but not found in the bug fixes or known issues list in v10.5. May i know there's a patch for v10.4 that resolves the issues?

These are the issue IDs in question:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

 

There are also some bugs listed in the compiler release note which remain to be un-resolved even in v10.7. May i know if there are plans to fix these issues?

These are the issue IDs in question:

MTWX26459

MTWX30211

 

Thanks. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,175件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport


Hi June.


Thanks for your reply.

here is more information:

ENGR00250596 : according to CCB decision, this feature was removed.

ENGR00184839 : Improve Error Reporting. Passed validation on MCU10.5 build B130625,

ENGR00243112: Passed in MU 10.5 b130701,

ENGR00252493: SA is not supported for simulators. Added filters for all simulator configs.  solved in CW10.5  build 131201.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,175件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi June

I can confirm there are no change for these two issue, for the moment, there is no plan to change them.

MTWX26459

MTWX30211

Regarding these four:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

Which version release note mentioned these issue? can you please upload the related doc. then I will check. Thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,174件の閲覧回数
June
Contributor I

Hi Jennie,

Many thanks for your reply. Regarding these issues:

ENGR00250596

ENGR00184839

ENGR00243112

ENGR00252493

They are mentioned in CodeWarrior Development Studio for Microcontrollers, v10.4 Release_Notes.pdf, Appendix A. I'm attaching the document here.

0 件の賞賛
返信
2,176件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport


Hi June.


Thanks for your reply.

here is more information:

ENGR00250596 : according to CCB decision, this feature was removed.

ENGR00184839 : Improve Error Reporting. Passed validation on MCU10.5 build B130625,

ENGR00243112: Passed in MU 10.5 b130701,

ENGR00252493: SA is not supported for simulators. Added filters for all simulator configs.  solved in CW10.5  build 131201.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信