Anyone know when there will be an IIC bean for the coldfi...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Anyone know when there will be an IIC bean for the coldfi...

ソリューションへジャンプ
2,499件の閲覧回数
freegeek
Contributor III
Anyone know when there will be an IIC bean for the coldfire V1.
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,192件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,
there are two I2C beans available in the CodeWarrior 6.0:

- The peripheral initialization bean Init_IIC allows a complete initialization of IIC peripheral but doesn't provide any runtime control, this is up to the user. This bean is available in all editions of CodeWarrior.

- The high level bean InternalI2C provides a comfortable setup and runtime use of the IIC device (sending characters, blocks etc.) However, this bean is a part of group called Advanced beans. License for these beans needs to be purchased separately - please contact your Freescale vendor for details.

best regards
Petr Hradsky
Processor Expert Support Team
UNIS


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,193件の閲覧回数
ProcessorExpert
Senior Contributor III
Hello,
there are two I2C beans available in the CodeWarrior 6.0:

- The peripheral initialization bean Init_IIC allows a complete initialization of IIC peripheral but doesn't provide any runtime control, this is up to the user. This bean is available in all editions of CodeWarrior.

- The high level bean InternalI2C provides a comfortable setup and runtime use of the IIC device (sending characters, blocks etc.) However, this bean is a part of group called Advanced beans. License for these beans needs to be purchased separately - please contact your Freescale vendor for details.

best regards
Petr Hradsky
Processor Expert Support Team
UNIS


0 件の賞賛
返信