908LJ12 - iam begineer - trying to load CW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

908LJ12 - iam begineer - trying to load CW

ソリューションへジャンプ
2,603件の閲覧回数
mohammed
Contributor III
Hi all
iam just tryen to use freescale controllers, iam very familier with PIC controllers and with Atmel controllers too, now i think i have to use freescale for cost issues,,,,,,,,
i tried to download CodeWarrior but my request rejected  - i don't know why-
 
now i don't know what to do, i need a compiler editor like MPLAB or Keil,
i just wanna use a sofware i can write assembly, and it tells me i write a wrong line
 
the problem is not bying the problem is trying,,,,,,,i need to try before i buy
 
iam intending to use 908LJ12 controller,,,,,,so any, any kind of help will be apretiated
1- i need compiler and debugger
2- i need samples for 908LJ12,,,, a very simple program; just make high and low on a pin -for now-

--
Alban Edit: Part Number must figure in subject line + subject line needs to be explicit
 


Message Edited by Alban on 2007-05-05 12:57 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,308件の閲覧回数
mohammed
Contributor III
thank alban
 
some how i downloaded the file from another link, CW V5.1, and it works fine
 
but there is a technical question, i'll put it in a new message

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,308件の閲覧回数
Alban
Senior Contributor II
Hello,

You can download CodeWarrior for HC08 from the following page:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247

It works and if you have problem downloading, I suggest you check your computer or with your ISP.

Regards,
Alban.


Message Edited by Alban on 2007-05-05 01:01 AM
0 件の賞賛
返信
1,308件の閲覧回数
mohammed
Contributor III
Hi Alban

thank you for the link, but i have tried to download that program before, but i failed;;;;;;;

the problem is they told me that you have to register first and after registeration a message comes

((((((Your request to download this item has been received and forwarded for review. A Freescale reprsentative will contact you.Thank you for your interest in Freescale. )))))))

and they send an email to me before. they said my request is rejcted without saying any reasons,,,,,,,,

i don't know why they do such thing,,,,,,,i have never seen that complications in downloading a demo version,,,

anyway i did it again,,,,and i made a new registeration......

please advice,,,,


best regards
hasan
0 件の賞賛
返信
1,308件の閲覧回数
Alban
Senior Contributor II
OK Mohammed, I don't understand why it would say this.

I move this thread to the CodeWarrior board and ask if someone could look at the system and check why you could not download it.
I don't know about download restrictions, except to certain countries written in the Terms of Use.

Cheers,
Alban.

0 件の賞賛
返信
1,309件の閲覧回数
mohammed
Contributor III
thank alban
 
some how i downloaded the file from another link, CW V5.1, and it works fine
 
but there is a technical question, i'll put it in a new message
0 件の賞賛
返信