908LJ12 - iam begineer - trying to load CW

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

908LJ12 - iam begineer - trying to load CW

跳至解决方案
2,511 次查看
mohammed
Contributor III
Hi all
iam just tryen to use freescale controllers, iam very familier with PIC controllers and with Atmel controllers too, now i think i have to use freescale for cost issues,,,,,,,,
i tried to download CodeWarrior but my request rejected  - i don't know why-
 
now i don't know what to do, i need a compiler editor like MPLAB or Keil,
i just wanna use a sofware i can write assembly, and it tells me i write a wrong line
 
the problem is not bying the problem is trying,,,,,,,i need to try before i buy
 
iam intending to use 908LJ12 controller,,,,,,so any, any kind of help will be apretiated
1- i need compiler and debugger
2- i need samples for 908LJ12,,,, a very simple program; just make high and low on a pin -for now-

--
Alban Edit: Part Number must figure in subject line + subject line needs to be explicit
 


Message Edited by Alban on 2007-05-05 12:57 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,216 次查看
mohammed
Contributor III
thank alban
 
some how i downloaded the file from another link, CW V5.1, and it works fine
 
but there is a technical question, i'll put it in a new message

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,216 次查看
Alban
Senior Contributor II
Hello,

You can download CodeWarrior for HC08 from the following page:

http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247

It works and if you have problem downloading, I suggest you check your computer or with your ISP.

Regards,
Alban.


Message Edited by Alban on 2007-05-05 01:01 AM
0 项奖励
回复
1,216 次查看
mohammed
Contributor III
Hi Alban

thank you for the link, but i have tried to download that program before, but i failed;;;;;;;

the problem is they told me that you have to register first and after registeration a message comes

((((((Your request to download this item has been received and forwarded for review. A Freescale reprsentative will contact you.Thank you for your interest in Freescale. )))))))

and they send an email to me before. they said my request is rejcted without saying any reasons,,,,,,,,

i don't know why they do such thing,,,,,,,i have never seen that complications in downloading a demo version,,,

anyway i did it again,,,,and i made a new registeration......

please advice,,,,


best regards
hasan
0 项奖励
回复
1,216 次查看
Alban
Senior Contributor II
OK Mohammed, I don't understand why it would say this.

I move this thread to the CodeWarrior board and ask if someone could look at the system and check why you could not download it.
I don't know about download restrictions, except to certain countries written in the Terms of Use.

Cheers,
Alban.

0 项奖励
回复
1,217 次查看
mohammed
Contributor III
thank alban
 
some how i downloaded the file from another link, CW V5.1, and it works fine
 
but there is a technical question, i'll put it in a new message
0 项奖励
回复