68HC908JB8: from Assembler CW2.1 to CW5 project conversion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

68HC908JB8: from Assembler CW2.1 to CW5 project conversion

Jump to solution
2,432 Views
marcom
Contributor I
Hi,
 
I need to convert this SW package:
 
 
from CW ASM2.1 to CW 5, so I can use all features of CW5.
 
In attachment the sw package.
 
Please help, I have find an application note, but is usefuless.
 
I think, that a CW *guru* can do this operation well, and explain how do this , so create a beautiful tutorial for this operation ?
 
Thanks
 
Marco 
 
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,254 Views
CrasyCat
Specialist III
Hello
 
The application note was for porting a CodeWarrior for HC08 V3.1 project to CodeWarrior for HC08 V5.x only.
 
What do you mean with CW ASM2.1? Which product is this?
Also are you using CodeWarrior for HC08 V5.0 or V5.1?
I assume your application is assembly only. Is it an absolute assembly project or a relocatable assembly project?
 
CrasyCat

View solution in original post

0 Kudos
Reply
1 Reply
1,255 Views
CrasyCat
Specialist III
Hello
 
The application note was for porting a CodeWarrior for HC08 V3.1 project to CodeWarrior for HC08 V5.x only.
 
What do you mean with CW ASM2.1? Which product is this?
Also are you using CodeWarrior for HC08 V5.0 or V5.1?
I assume your application is assembly only. Is it an absolute assembly project or a relocatable assembly project?
 
CrasyCat
0 Kudos
Reply